EXTENCODER.POSITION

Description

Gets the external encoder (EEO) position.

General Information

Type

R/W

Units

1/(2^64)

Range

-2^63 to +2^63 -1

OR

0 to EXTENCODER.POSMODULO

Default Value

0 Counts

Data Type

Integer

Variants Supported

This parameter is only supported on AKD BASIC drives.

Fieldbus Information

Fieldbus

Index/Subindex

Is 64 bit? Attributes Signed?

Object Start Version

Modbus

1080

Yes 64 bit Yes

M_01-05-11-000